CMP#.MODEN

Description

CMP#.MODEN turns the modulo function for the compare channel on or off.

Examples

Usage

0: Turn modulo off (default)

1: Turn modulo on

Code

These commands turn modulo on for channel 1 and off for channel 2.

--> CMP1.MODEN 1
--> CMP2.MODEN 0

Context

See Compare Engines View.

Versions

Action Version Notes
Implemented 02-06-00-000  

General Information

Type

Read/Write

Units

N/A

Range

0 to 1

Default Value

0

Data Type

Integer

See Also

CMP#.MODVAL1, CMP#.MODVAL2

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

CMP1.MODEN

4500h

02h

Unsigned8

-

-

Read/Write

No

CMP2.MODEN

4501h

02h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

31520

1

31520 (0x7b20)

CMP1.MODEN

Unsigned8

Read/Write

Yes

31521

1

31521 (0x7b21)

CMP2.MODEN

Unsigned8

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

CMP1.MODEN

31520

Unsigned8

Read/Write

-

CMP2.MODEN

31521

Unsigned8

Read/Write

-